Your message has been sent, you will be contacted soon
Keysight

Call Me Now!

Close
Home » news » Solution for Triggered Acquisitions at Fast Rate without Missing any Events

Solution for Triggered Acquisitions at Fast Rate without Missing any Events

We announced today, on Keysight newsroom, the availability of new signal processing firmware for our family of U53xxA PCIe digitizers. The new firmware (option -TSR) allows simultaneous capture and transfer of acquired data in triggered applications.

According to our validation measures, the digitizer’s architecture, with the new firmware, is able to sustain triggered acquisitions of thousands of samples at hundreds of kHz rates without missing any events. Moreover, with the new firmware, it is possible to acquire and read substantially higher trigger rates during a shorter period of time (or non-periodic triggers) depending on the internal memory options selected. Users now can view the memory as a multi-bank circular memory, and can optimize the data throughput for their application by configuring the number of memory banks.

“The -TSR option offers an optimum solution for triggered applications that require a large volume of data transfer while making sure none of these triggers are missed,” said Jean-Luc Lehmann, product manager for Keysight PCIe high-speed digitizers. “This new function enlarges the coverage of OEM needs once more. Other specific functionalities, such as real-time peak detection and average, are already available.”

About Benedetta Viti

Benedetta is a PR & Web Editor. She is the key player behind the blog High-Speed ADC, willing to know more about the people behind the products. She holds a Bachelor in Languages and a Master in International Marketing.

Leave a Comment